CyberPower Systems Launches a Next Generation FTTx DC Desktop Power Supply & Battery Backup Units

March 6, 2012 by CyberPower

CyberPower Systems, a leading technology manufacturer in the FTTx DC power supply industry, today announced the introduction of its new line of Desktop FTTx DC power supply and battery backup units, Models DT30U12V-NA3 and DT30U12V-NA3-G. Designed for mountable locations and desktop use, these units are ideal for installations inside the home as opposed to more traditional or outdoor locations. This flexibility allows for flexibility of location and reduced installation costs, benefiting both telecom providers and home users.

These units are like no other in the industry, in that they are aesthetically pleasing and have a flexible design, which allows the unit to be installed in the home on desktops as opposed to other more remote, out-of-sight locations such as garages, basements, utility closets, or other out-of-sight locations. This flexibility allows telecom providers to install the devices faster and in plain sight where the units can be positioned with other devices such as phones, cable modems, broadband routers and other home electronics. This makes wiring faster and cuts down on installation costs. “The new, cost-effective FTTx DC Power Supply and Battery Backup is a compact design, brings the advanced features previously only available to the RBOCs to any service provider in an aesthetically pleasing, customer friendly design.”, says Mark Lewis, Senior Engineer at CyberPower Systems. “We’re excited about this product introduction, as we’re the first in the industry to manufacture a product with this rich a feature set, for all levels of a service provider.” In addition to offering these as stand-alone solutions, Telecom providers can now bundle these with their cable and telephone triple-play or multi-service packages, making these an ideal solution for any telecom company looking to offer a wider array of services at more affordable price points.

In addition to a more compact, flexible design, the units feature an advanced LED and audible indicator system with six control devices for simple customer interpretation of unit status. The improved battery algorithm accurately tests and maintains the battery for peak performance with minimal degradation, and allows for the greatest utilization of battery capacity. The alarm can be muted with the systems’ ALARM SILENCE technology, enabling users to selectively silence the audible alarm for up to 24 hours or indefinitely. To activate reserve battery power or to start the units with a new battery, users can press the COLD START button, allowing extended use of the unit.

The units have an input voltage range of 100Vac — 240Vac with a frequency range of 47 — 70Hz. The on-battery output voltage is 12Vdc nominal and runs with continuous power capacity of 30 watts and greater than 75% efficiency. The unit utilizes a commonly available 12V 7.2AHr battery.

To learn more about CyberPower Systems’ FTTx solutions, visit www.cpsww.com or call (877) 297-6937.