CyberPower Systems, the global leader of innovative power protection and distribution equipment, today announced the addition of its CP350SLG Standby Series uninterruptible power supply (UPS). It safeguards PCs, personal electronics, POS equipment, and security/surveillance systems from blackouts, brownouts, surges, spikes, sags, and other power abnormalities. Advanced lightning protection is attained with composite integrated circuitry. The CP350SLG UPS has a capacity of 350VA/255Watts with six NEMA 5-15R receptacles, including two widely-spaced outlets to accommodate transformer-based plugs. Protection for phone/network (RJ-11) is also provided.
Read the full press release.