Prevents accidental electrical shock by blocking foreign objects from entering the open spaces with internal shutters.
Need help with TR outlets? See our FAQ
—Common CyberPower phrases and terms.
Prevents accidental electrical shock by blocking foreign objects from entering the open spaces with internal shutters.
Need help with TR outlets? See our FAQ
Saves energy by reducing the amount of standby energy used by desktop computers, home theater AV equipment and plasma or console style television sets. These power strips have three types of outlets: master, always-on, and energy-saving. These power strips also include surge protection to divert excess voltage away from electronic equipment during a power surge to prevent damage to sensitive electronic equipment.
Reduces energy consumption by using an infrared (IR) smart sensor to shut down all home theater devices when the television remote has not been used for one or two hours. These power strips also include surge protection to prevent damage to sensitive electronic equipment by diverting excess voltage away from the television and connected devices during a power surge.
The process of dissipating heat from an electrical system via air or liquid cooling. Also, a term for the amount of heat a device can emit.
Reduces heat and improve UPS battery life up to five years with the Smart Battery Management (SBM) charging system.
Covers defects in materials and workmanship in the product under normal use and conditions within three years of the purchase date. See warranty for details.
CyberPower will repair or replace a defective UPS system (including batteries) within three years of the purchase date. See warranty for details.
A calculated measure of the distortion in sine wave clarity caused by higher wave frequencies.
The time it takes UPS to switch from AC power to battery power.
A device that converts AC line voltage to a higher or lower value.
Accommodate large transformer-based plugs without compromising the access of other outlets.
Secures an outlet by twisting and locking into place to prevent accidental disconnection.
Explore product guides, manuals, publications, and more
Frequently asked questions from CyberPower users like you
Recent CyberPower recalls and critical notices