Communications Between the UPS and Maintenance Bypass PDU
CyberPower Maintenance Bypass PDUs with an MBP Detection Cable can communicate directly with the UPS to safely coordinate the bypass switch operation. When the PDU bypass switch operation is initiated by removing the cover, the MBP Detection Cable sends a signal to the UPS to internally transfer to bypass mode to prevent damage.