Rack mount depth is commonly confused with the overall rack depth including the door. Mounting depth is defined as the dimension from the front of the front rack angle to the back of the back rack angle. Many racks have adjustable mounting depth so it’s best practice to ensure that the rails being used for all the equipment will fit the depth of the rack. The most common depth is between 28″-29″.
Questions?
Talk to a specialist
1.877.297.6937