The red battery power LED will be lit. If this LED not lit, then slide the switch to the battery position.
Questions?
Talk to a specialist
1.877.297.6937
We are having issues with Support Ticket Submissions. Please use the "Let's Chat" or call 1-877-297-6937 to connect with support while we resolve this issue.
—FAQs
1.877.297.6937
The red battery power LED will be lit. If this LED not lit, then slide the switch to the battery position.
Yes, all switched metered-by-outlet PDUs also monitor and display input/circuit power readings.
Firewire or FireWire® Cable is also known as IEEE 1394. The original release of IEEE 1394-1995 is now known as Firewire 400. It can transfer data between devices at 100, 200, or 400 Mbit/s. The cable’s maximum length is limited to 14.8 ft. (4.5 meters), but you can have up to 16 cables daisy-chained by using active repeaters, external hubs, or internal hubs.
Install and run the power device network utility software. Once open, click on the underlined IP address to login. Once logged in, click on the System tab and select Network Service. On the next screen double click your PDU’s MAC address. This will direct you to the Device Setup screen so you can set a Read More ›
Use Agent when you are connecting the computer to the UPS with a USB or Serial cable. Use Client if you are connecting the computer via your network to the RMCARD installed on the UPS. Use Center when you want to monitor and manage all the CyberPower power protection products on your network.
Username: cyber Password: cyber
For PDUs with a display screen: Press and hold the select button for a few seconds. Once “IP” appears on the display screen, release the button. Your unit will then display the IP address in a sequence of four groups. For example, the IP address 192.168.20.177 would begin by showing 192, then 168, the 20 Read More ›
CyberPower pays for shipping when we send items to you. You pay for shipping when you send items to us. Pack and ship the product to CyberPower and, if requested by us, the item(s) of connected equipment, along with all the claim forms that we provide to you. Show the claim number on the shipping label or include it with the product.
Yes, all switched metered-by-outlet PDU models can be configured via the web management interface.
Contact Technical Support for assistance with installation, troubleshooting, and answers to questions about your CyberPower product.
CyberPower switched metered-by-outlet PDUs provide device-level and circuit-level monitoring of input power (V), input frequency (Hz), load (A, kW, kVA), peak load (A) and energy usage (kWh); and outlet-level monitoring of load (A, kW), peak load (kW) and energy usage (kWh).
We recommend that you promptly register the product you purchased. You may register online by clicking the Registration button at the top of the page.
Explore product guides, manuals, publications, and more
Learn more about warranties and register your product
A-to-Z definition guide for common CyberPower phrases and terms
© 2025 Cyber Power Systems (USA), Inc. CyberPower is a registered trademark and brand of Cyber Power Systems (USA), Inc. All rights reserved.