Yes, with the optional EnviroSensor installed and connected. The EnviroSensor will monitor ambient temperature and humidity and report that information to the PDU.

Questions?
Talk to a specialist
1.877.297.6937
—FAQs
1.877.297.6937
Yes, with the optional EnviroSensor installed and connected. The EnviroSensor will monitor ambient temperature and humidity and report that information to the PDU.
Yes. All CyberPower power inverters will beep when they are turned on or restarted.
This is due to overloading the unit. You will need to reduce the load placed on the unit or purchase a larger unit.
This is due to overloading or underpowering. Overloading is caused by an excessive load and can be resolved by either upgrading to larger power inverter or by reducing the load of the attached equipment. If the device is underpowered, connect it to power source that is outputting greater than 11 volts. Most often, users simply need to start their vehicle and recharge the battery.
Many airlines limit in-seat power to a maximum of 75 watts. (Most laptops require >100 watts.) The recommended workaround is to remove the battery from the laptop. Doing so should reduce the power demands of the laptop to under 75 watts because the battery will no longer be charging while the laptop is in use.
If your unit is within the warranty period, you can receive a free replacement from CyberPower.
If your unit is within the warranty period, you can receive a free replacement from CyberPower.
Indoor design provides durable casing to protect an FTTx/Telecom unit.
Outdoor design provides outdoor mounting and durable, weather-proof casing to protect an FTTx/Telecom unit.
Yes, switched PDU models can be configured via the web management interface.
Metered, monitored, and switched PDU models display the total current being drawn by the connected equipment on the screen. If there are two outlet banks, then the display is showing the total aggregate current draw between both banks.
Yes, PowerPanel Business Edition can be installed on a computer to configure unattended shutdown settings. For details, please see the PowerPanel Business Edition User Manual.
Explore product guides, manuals, publications, and more
Learn more about warranties and register your product
A-to-Z definition guide for common CyberPower phrases and terms