Filter by Topic
Show Filters
All Frequently Asked Questions
What is the standard rack vertical hole spacing?

Vertical hole spacing is defined as a repeating pattern of holes within one rack unit (RU or U) of 1.75″. The hole spacing alternates at 1/2″ – 5/8″ – 5/8 and repeats. The start and stop of the RU is in the middle of the 1/2″ spaced holes.

Should the cooling fan on my CyberPower UPS be running at all times?

The internal cooling fan will only run when it is required. CyberPower UPS systems utilize an internal thermometer which activates the fan when the temperature exceeds a certain threshold. When the UPS is running idle (not using battery power), it is completely normal for the fan to not be running. The exception is with Online units, models that begin with “OL”. Their cooling fans will run ALL the time.

How do I dispose of my UPS?

CyberPower Systems encourages environmentally sound methods for disposal and recycling of its UPS products. Please dispose of and/or recycle your UPS and batteries in accordance to the local regulations of your state.

If my surge protector has a ground light, should it be illuminated (green)?

Yes. The ground indicator light should be illuminated. If the light is not illuminated, there is a problem with the AC outlet into which the CyberPower surge suppressor is plugged. If this is the case, please disconnect the surge suppressor until the problem is resolved. The problem must be resolved before the CyberPower surge suppressor can be used.

If my surge protector has a surge light, should it be illuminated?

Yes. The surge light should be illuminated. This indicates that the CyberPower surge suppressor is functioning properly. If the light is not illuminated, it indicates that the surge protector has received a catastrophic surge and will need to be replaced. CyberPower will replace the surge suppressor free of charge, provided the warranty terms and conditions are met.

How do I run a self-test?

To run a self-test, open the Power Panel software and then click “Initiate Self Test”. Another way to perform a self-test is by turning off the circuit breaker for the circuit the UPS is plugged into or unplugging the unit from the wall.

More Resources