Yes, however, the LCD panel will be easier to use when the UPS is in its standard orientation. If you choose to position the UPS unit in a non-standard position, make sure the fan on the back and at least one of the side vents are left unobstructed so the UPS has plenty of airflow.

Questions?
Talk to a specialist
1.877.297.6937