Yes, the User Manual for the CyberPower Remote Management Card that is used for the RMCARD205 and RMCARD305 can also be used for the Gigabit RMCARD.

Questions?
Talk to a specialist
1.877.297.6937
—FAQs
1.877.297.6937
Yes, the User Manual for the CyberPower Remote Management Card that is used for the RMCARD205 and RMCARD305 can also be used for the Gigabit RMCARD.
If the power feed is protected upstream, by an appropriately sized overcurrent protection device, an input circuit breaker is not required. If the output is feeding a distribution panel with a properly sized main circuit breaker, the output breaker is not required. With all of that said, having the circuit breakers located at the UPS Read More ›
If N+1 is purchased, YES! If your system is not configured for N+1, each power module supplies 10KVA of power, so if you are running 20KVA of load on a 40KVA system you can swap power modules because the system will remain running on 30 of 40KVA, easily picking up your 20KVA load until the Read More ›
Redundant redundancy, for the most critical applications. Two N+1 UPS systems in parallel to increase reliability exponentially and eliminate downtime. Provide confidence that you are prepared for the unexpected.
N+N is a second complete UPS wired in parallel, distributing 50% of the load evenly across the two units. If one UPS were to fail, the load would be seamlessly picked up by the reciprocal UPS.
N = Power delivered by the UPS (e.g. 20KVA). +1 refers to an extra power and battery module for redundancy. If there is a fault in one module it can be replaced while still providing fully protected power.
Please call for pricing and availability.
CyberPower Medical Grade Power Protection Products have been designed to tolerate repeated cleaning in healthcare environments. CyberPower Medical Grade UPS Systems are safe to clean with products containing the chemicals listed below in the concentration specified or less: APPROVED CLEANING CHEMICALS: Ethyl Alcohol 75% Isopropyl Alcohol / Isopropanol 75% Hydrogen Peroxide 5% Sodium Hypochlorite 12% Read More ›
Laser printers use a very high amount of power and can easily overload your UPS. Overloads of this type can damage your UPS. As such we ask that you do not plug laser printers in to the battery backed outlets of the UPS.
The Automatic Voltage Regulation (AVR) in UPS systems adjusts the incoming AC voltage to stabilize the output power to connected equipment.
What is the Wiring-Fault Indicator Light?
The LED indicator will illuminate red to warn the user that a wiring problem exists, such as bad ground, missing ground or reversed wiring.
Explore product guides, manuals, publications, and more
Learn more about warranties and register your product
A-to-Z definition guide for common CyberPower phrases and terms