CyberPower has released an update to the Smart App Sinewave UPS, models PR3000RTXL2UAC and PR3000RTXL2UHVAC. See what is new in the notes below and download.
For UPS Smart App Sinewave UPS models PR3000RTXL2UAC and PR3000RTXL2UHVAC. Firmware version 1.1786 (US Release Date: 09/20/2024)
Fixes
- Resolves an issue where the installed RMCARD205 will not display the correct number of EBMs attached. The RMCARD205 will show one less EBM than is attached.
- The number of EBMs and Run-time will be displayed correctly on the UPS control panel
- The issue does not affect performance or run-time
- The updated UPS firmware will correct the information displayed on the installed RMCARD205
Questions? Contact Tech Support Monday through Friday from 7am– 6pm cst.
Download link and release notes are available here:
https://www.cyberpowersystems.com/products/software/firmware/