CyberPower Smart App Online Series UPS systems include a Generator Mode setting specifically designed to work with generators. With varying loads, the frequency output from generators can be erratic. This erratic output can make it difficult for a UPS without a Generator Mode setting to recognize the input power, causing the UPS to function on battery power only. With Generator Mode, the UPS can automatically adjust to frequency fluctuations and maintain a full charge of the batteries.
![LCD Control Panel](https://dl4jz3rbrsfum.cloudfront.net/images/feature-focus/ol-lcd-generator-mode.jpg)
See also Generator Compatible.